Other Parts Discussed in Thread: DLPC3436,
Dear Sir/Madam,
We have purchased the DLPDLCR230NPEVM, and we tested it using a power supply: 5V 5A. The spec on page 6 paragraph 4 states that when you power up the EVM it will display a logo. Also that the the D_HOST_IRQ will be OFF ( which indicates a successful boot of the DLPC3436), and that the D_DONE and D_INIT_B will be ON (to indicate a successful boot-up of the FPGA). However the D_HOST_IRQ is constantly On, and the D_DONE goes On and Off and the image flashes momentarily. Does that mean that the FPGA and the DLP3436 have failed? please advice.