Dears:
DLPA3000DPFD/DLPC350ZFF are both operation temperature Ta is zero above, whether it can work at zero temperature below as 20 degrees below zero, if not, can you help to promote industrial grade PN instead of the both.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
DLPA3000DPFD/DLPC350ZFF are both operation temperature Ta is zero above, whether it can work at zero temperature below as 20 degrees below zero, if not, can you help to promote industrial grade PN instead of the both.
Hello Cooper,
Welcome back to the E2E forum and thank you for your interest in DLP technology.
I am a bit unclear on your question. The DLPC350 has an operating junction temperature range from 0 to 105 degrees Celsius as described in section 6.3 (page 14) of the DLPC350 Datasheet.
If this is meant for a general display application, you may consider using a DLPC3430 or DLPC3433 which are rated to work down to -35 degrees Celsius.
Regards,
Austin