This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500NIR: MWIR Options?

Part Number: DLP4500NIR

Upon reviewing the current DLP offerings it appears the limiting factor for working with Mid-IR (2 - 5um) is the window material. 

1. Does the DLP product roadmap include any future consideration for Mid-IR wavelengths?

2. I understand from reading an earlier post that the window can NOT be removed without destroying the device.  Does TI provide any customization options for customers, for example changing the window to sapphire?

  • Hi Patrick,

    1. At this point, we don't have MWIR our roadmap. Doesn't mean it won't change in the future however.

    2. Unfortunately not. Manufacturing the DMD is quite complex and it is not a simple matter to customize the device.

    Hope that answers your questions!
    -Paul