Other Parts Discussed in Thread: DLP7000
Hi,
I have a question about the refresh rates of DLP7000UV. I understand that it is 32kHz for a single bit. Does it mean that to change all the pixels for a 1024x768 device, it takes about 24 seconds (number of pixels divided by single bit refresh rate)? Or individual mirrors can be addressed in a parallel fashion and that the entire array can be refreshed at a rate of 32kHz. Sorry if the question is a bit naive, I am quite new at this technology.