This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP650NE: Using DLP650NE without using the DLPC4422 controller

Part Number: DLP650NE
Other Parts Discussed in Thread: DLPC4422,

Hello.

1. I am looking to see if there is a way I can use the DLP650NE without using the DLPC4422 controller?

2. Also, in order to operate the DLP650NE, I see that the DCLK is 400 MHz and there are two other control signals associated with it is SCTRL_AP and SCTRL_AN. Are these 2 control signals SCTRL_AP and SCTRL_AN are required to drive the 64 bit LVDS input to the DLP650NE? 

3. What is the state of these 2 control signal SCTRL_AP and SCTRL_AN?

Thanks,