Can I use the DLP 7000 UV with Quartz window customization ?. Is TI giving with various glass window options?.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Satish,
At this time we do not support custom windows for the DMD. In addition there are other reasons apart from the window transmission that we do not support wavelengths below 363 nm. Please see this application note:
System Design Considerations Using TI DLP® Technology in UVA (363 – 420 nm)
Best regards,
Fizix
Satish
Can you share more details on what you are looking for?
you can contact me directly through an E2E friend request if you do not want to post in a public forum