This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: Technical Spec DLPC410, DLPC900, DLPC910, DLPC4422

Part Number: DLPC900
Other Parts Discussed in Thread: DLPC410, DLP7000, DLP9500, DLP650LNIR, , DLP9000, DLPC910, DLP9000X, DLPC4422, DLP660TE, DLP470TE

Hello,

Could you please help-me trying to fill correctly the values on the next table?

Empty cells are because I didn't find the values on the datasheets. 

"Bus" with red values, I didn't understand what it means and what is the relation between LVDS, 2xLVDS, 16-bit...

Are "Bus", "Clock/Row" and "Data Lines" related between them?

Controller Clock DMD Columns Rows Blocks Rows/Block Data Lines Clocks/Row Bus
DLPC410 400 MHz DLP7000 1024 768 16 48 32 16 2x (2xLVDS) 16-bit
DLPC410 400 MHz DLP9500 1920 1080 15 72 64 16 4x (2xLVDS) 16-bit
DLPC410 400 MHz DLP650LNIR 1280 800 16 50 16 40 2x (LVDS) 16-bit
DLPC900 400 MHz DLP6500 1920 1080 15 72 2x (2xLVDS) 16-bit
DLPC900 400 MHz DLP9000 2560 1600 16 100 4x (2xLVDS) 16-bit
DLPC910 400 MHz DLP6500 1920 1080 15 72 32 2x (2xLVDS) 16-bit
DLPC910 400 MHz DLP9000X 2560 1600 16 100 20 4x (2xLVDS) 16-bit
DLPC4422 DLP660TE 3840 2160 4x (2xLVDS) 16-bit
DLPC4422 DLP470TE 3840 2160 4x (2xLVDS) 16-bit

Thank you so much,

Cédric Pereira

  • Hello again Cédric,

    Please allow a little time for me to make sure that I provide correct numbers.  Probably tomorrow (may 14) afternoon.

    Fizix

    P.S.  I accidentally marked this as "TI thinks resoved".  Ignore that until I get this filled out.

  • Of course! Thank you for your interest! :)

  • Hello,

    Sorry, when is it possible to get some feedback?

    I would like to finish a review on Tuesday.

    Thank you,

    Cédric Pereira

  • Hello again Cédric,

    I was attempting to find out about the DLP660TE and DLP470TE.  The information you requested on those devices is not published.  Since they are video controller chips, this is taken care of my the DLPC4422 controller.

    Here is the table [N/S = not shared]:

    Controller Clock DMD Columns DMD Rows Blocks Rows/Block Data Lines Clocks/Row Bus

    DLPC410 400 MHz DLP7000 1024 768 16 48 32 16 2x (2xLVDS) 16-bit
    DLPC410 400 MHz DLP9500 1920 1080 15 72 64 16 4x (2xLVDS) 16-bit
    DLPC410 400 MHz DLP650LNIR 1280 800 16 50 16 40 2x (LVDS) 16-bit
    DLPC900 400 MHz DLP6500 1920 1080 15 72 32 32 2x (2xLVDS) 16-bit
    DLPC900 400 MHz DLP9000 2560 1600 16 100 64 20 4x (2xLVDS) 16-bit
    DLPC910 400 MHz DLP6500 1920 1080 15 72 32 32 2x (2xLVDS) 16-bit
    DLPC910 480 MHz DLP9000X 2560 1600 16 100 64 20 4x (2xLVDS) 16-bit
    DLPC4422 400 MHz DLP660TE 3840 2160 N/S N/S 64 N/S 4x (2xLVDS) 16-bit
    DLPC4422 400 MHz DLP470TE 3840 2160 N/S N/S 64 N/S 4x (2xLVDS) 16-bit

    Fizix

  • Thank you so much!

    My best regards,

    Cédric Pereira