Part Number: DLPC900
Other Parts Discussed in Thread: DLP6500FYE
Hi,
DMD can't light up after power on.
HW: DLPC900 + 6500 No HDMI. DMD chip inspection is normal (using EVM).
DMD Board: 3.3V Power rail is normal
EN_OFFSET pin : 0V (Without dmd and power up to 3.3v VOFFSET / BIAS / VRESET is work fine)
DLPC Debug Log:
[2021-01-06 10:29:34.135]# RECV ASCII>
Bootloader Version 3.0
Jumping to application ...
Debug opened on URT0
Memory test cc = 1
API version: 05.00.01
App version: 05.00.01
Configuration layout versions:
Seq Map: 44.21.0100
SW Map: 44.21.0000
I2C Cmd Slave Address 34
[2021-01-06 10:29:39.596]# RECV ASCII>
DRAM memory pool 004025E8 200025E8
[2021-01-06 10:29:39.692]# RECV ASCII>
ptn_seq.c (1014) >> Failed
Illumination: Transition to operating mode
DMD comm error in DMD_Power()
Illumination: Transition to standby
Measure the following IO status (connected to dmd chip):
PWRDNE + RESETZ : 3.3V
RESETZ_OEZ: 3.3V
RESET_IRQZ: 0V (Without DMD 3.3V)
Looking forward to your reply
best regards
Byron