Part Number: DLP470TP
Hello Team,
My customer is developing an aerospace camera. The idea was to use the microdisplay as an object in the focal plane of a collimator, and use the collimated beam to illuminate the camera with images at "infinity" to test the camera in close to real conditions. They need a high resolution (4K) display, and they think DLP470TP can be used to it.
But some doubts on how it works, is the image obtained by the DLP microdisplay is already collimated? so in that case, could they directly project it into our camera without the need of using a collimator?
How are the images provided to the DLP? Is there any controller associated with it?
Can they provide the images using standard software or is it necessary for any additional software?
Regards,
Renan