Hi Team,
I downloaded version 4.0.0 of "DLP LightCrafter 4500 EVM GUI - Windows" and compiled it with 64 bit QT. There was a compilation error. Finally, I uninstalled 64 bit QT and compiled with 32-bit QT successfully. Now I need to migrate version 4.0.0 to Linux system. Then I want to ask if I need to install 32-bit QT in Linux system? But the important thing is that I can't find the 32-bit QT of Linux after 5.0 version on the Internet so I can only download the 64 bit QT.
Beat Regards,
Tom Liu