Other Parts Discussed in Thread: DLPC3479, DLP2010LC, DLPC3470, DLP2010, DLPC3478
Hello!
We are successfully using two LightCrafter 6500 modules in a neuroscientific visual stimulation setup. We want to build another similar third setup but unfortunately the LC6500 is not available anymore. Thus, I am now looking for a replacement module.
It is important for us is:
- the module allows pixel accurate presentation of the provided video stream (like the “video pattern mode” on the LC6500 with the pattern stream provided by HDMI or DP)
- the module has a precise frame-wise trigger out
- the module allows high 8-bit greyscale framerates (>= 120 Hz) in pattern mode
In my own research on your modules I found the DLP4710EVM-LC which apparently meets our criteria. It seems to allow 180 Hz 8 bit video pattern mode.
Could you confirm the latter? Are there other module with similar or better specs?
Thanks a lot for your support!
Best,
Malte