This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA2000: PG failure

Part Number: DLPA2000
Other Parts Discussed in Thread: DLPC3433, DLP3010

Hello,

I am trying to boot a custom board with the  DLPA2000 and DLPC 3433. I have no success so far. The IRQ signal from the DLPC3433 remains high, and I note that the LS_OUT of the DLPA 2000 is under 1.3v (around 1.299v). This is specified in the datasheet as a PG Failure. How could I discover the origin of the failure?. Is it only related to thermal detection or to some undervoltage? Setting up PROJ_ON/OFF again has not solved the issue.

Thanks