Hi E2E,
Good day.
Our customer is using a light engine with DLPC900 chipset. They would like to use either pattern-on-the-fly mode or pre-stored pattern mode to run 10,000+ patterns. However, they cannot load more than 50 patterns with 8-bit depth to the onboard storage using pattern-on-the-fly mode. Is there any method to run pattern-on-the-fly without loading them to onboard memory so that they can run 10,000+ patterns?
Regards,
Carlo