I have problem with connecting with DLP lightcrafter 4500 and computer.
- I am using a 12V 5A power supply, but it is expected to be 12V 6A
- I am using DLPLCR4500 GUI 4.0.0
- I checked c184 ~1.2V and c71 ~3.2V (https://e2e.ti.com/support/dlp/f/dlp-products-forum/651321/dlpc350-light-crafter-4500-evm-doesn-t-connect-via-usb-red-led-on-back)
- The red light and green light both show up
- J18 and J30 I tired jumper but nothing happening. (https://e2e.ti.com/support/dlp/f/dlp-products-forum/306191/dlp4500-can-t-connect-to-the-computer)
- computer does not even recognize the device, I do not see anything from device manager.
Easy solution : return it and get a new one.
https://e2e.ti.com/support/dlp/f/dlp-products-forum/329341/dlp4500-can-t-quickstart-nor-connect-usb
Any suggestion?