Hello!
1.
What are the differences between firmware dlpc3470 8.0.0 (latest version) and firmware 8.0.0_RED_LED_ONLY?
2.
Where can I see the state graph of micromirrors for firmware 8.0.0_RED_LED_ONLY?
Vladimir.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
1.
What are the differences between firmware dlpc3470 8.0.0 (latest version) and firmware 8.0.0_RED_LED_ONLY?
2.
Where can I see the state graph of micromirrors for firmware 8.0.0_RED_LED_ONLY?
Vladimir.
Zhukov,
The main difference between the standard firmware and "RED_ONLY" firmware is that the "RED_ONLY" firmware boots with the BLUE and GREEN LED channels disabled in the PMIC. This means that in hardware these LEDs can be disconnected with only the RED channel connected without causing any current drive issues for the system.
Nothing else about system operation (video data, DMD operation, etc.) is changed.
Regards,
Philippe