I want to communicate with my DLP Lightcrafter 4500 with NI LabVIEW. Lightcrafter 4500 comes with the DLPC350 controller. According to the DLPC350 Programmer’s Guide there are two methods to interface with DLPC350; USB, and I2C.
Other posts in this forum that shared a method to interface with LabVIEW or MATLAB implied they had a different controller (DM365) which communicates with a PC using TCP. Two example posts are: MATLAB code to control LightCrafter(TM) and DLP LightCrafter Labview