Other Parts Discussed in Thread: DLP6500FYE,
I'd like to use the 6500FLQ chip, not the FYE chip for my project, I need the response down to 400 nm that the FLQ has. Is it possible to get the FLQ chip mounted on the 6500EVM board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'd like to use the 6500FLQ chip, not the FYE chip for my project, I need the response down to 400 nm that the FLQ has. Is it possible to get the FLQ chip mounted on the 6500EVM board?
Hello Jim,
The DLP6500FLFQ will not directly mount to the EVM DMD board. The EVM DMD board is designed for the DLP6500FYE DMD which has pins on the back and the DLP65000FLQ has pad on the back which is used in conjuntion with a "C-spring" interposer to make a positive connection between the DMD pads and pads on a DMD board of your design.
You may want to check with some of our design partners to see if they already have a DLP6500FLQ DMD board designed.
You can find them from links on the following page:
http://www.ti.com/dlp-chip/support-training.html <-- check the different link groups, especially the "DLP Design Network".
Fizix