Is there any built-in timeout for the TI Lightcrafter when communicating through TCP/IP ? The device seems to stop communicating with the PC after a 5-10 mins. The only get it to work again is to do hard reset on the Lightcrafter. This also happens when using the GUI program from TI.
Also, the device seems to take an arbitrary amount of time (sometimes a very long delay) before we can establish a connection after starting/restarting the device. We just have to keep clicking on the "Connection" button in the GUI and wait for it to respond.