The workaround mentioned below applies to USB connection issues (when LightCrafter is connected to PC via USB) like code 10 error, corrupted RNDIS driver, 'USB device not regonized' or if you notice 'unknown device' under Universal Serial Bus Controllers in Device Manager.
please follow the below procedure in specified order,
- Uninstall the RNDIS driver ( if its already installed). To uninstall, go to Device Manager (Control Panel -> System -> Device Manager) and remove the networking entries for RNDIS. Look under Network Adapters, select RNDIS/ Ethernet Gadget and right-click uninstall.
- Disconnect the LightCrafter from PC (and power off the LightCrafter)
- Disable all the network connections(even WiFi)
- Reboot the computer and wait for a complete start up
- Power up the LightCrafter and wait for the vertical color bars to display
- Connect the LightCrafter to the PC via USB to the new/ different port on the PC
- Auto install the driver as instructed in the DLP LightCrafter's User's Guide (link )
- Wait for the installation and network address assignment to complete
Connecting a USB hub in between the PC and cable also resolves the issue.