Hi,
we're controlling the Lcr using the USB/RNDIS interface. We've developed our own code for this operations, and it is working as intended. The problem we´re facing right now is the speed of this comunnication, since our application uses the Patter Sequence projection at almost the max speed.
In the Light Crafter's User's Guide the following is sayed, but that's all I've found about UART communication:
"DLP®LightCrafter™’s UART port serves as a console output of the embedded Linux device. The DM365 will send error messages through the UART and accept root level commands. A 2.5 mm stereo plug to female DB9 connector as shown below is needed to connect the DLP®LightCrafter™’s UART port to a PC. "
Which are those root commands?
Is there more information available about the UART communication?
Are there examples available?
Is there any other way of communicating with the Lcr besides UART and USB/RNDIS?
Thanks