This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LightCrafter Version2.0 - What is the difference?



Dear All,

I got new LightCrafter today from TI. It  is labeled as "Versoin 2.0". But my another LightCrafter(which was obtained at early 2012) seems not to be "Version 2.0".  What is the difference between the "Version 2.0" and the previous version?

Thank you and best regards,

Rossinag

  • Dear Rossinag,

    The DM365 software  v3.31 and above has additional Extended Pattern Sequence mode which allows to load patterns from SD card. This features requires a GPIO connection with NAND and hence R205 is installed on v2.0 Boards.

    The USB transient suppressor part is also changed on the v2.0 systems board to enable USB 2.0 connection.

    Regards,

    Divya

  • Hello Divya,

    Thank you for your description. I understood.

    Indeed, the USB connection is stable.

    Thank you and best regards,

    Rossinag