Hi,
I am trying to use the LightCrafter 4500 with external LEDs.
As such I have unplugged the LEDs and reconnected the DMD to the board without the lightengine (as in the image below)
.
I then connected the board to a 12 V supply neglecting to connect the J30 jumper. After about 30 seconds of operation (and a concerning vibrating sound) a thin band appeared on the DMD. It can be seen the figure above and upon re-projecting the logo image it can be seen in the image below.
Inside this band (neglecting inversion) I have good contrast but outside I have poor contrast. If I do a forced swap from video mode to the pattern sequence in the GUI the image freezes to a high contrast image. So high contrast is achievable (but through a glitch).
Question 1: If I run a sequence with a long exposure time (as bellow) would I expect with a normal operating unit a high contrast image on the DMD? (the micro-mirrors being fixed to either + or - 12 degrees?)
Question 2: What is causing this contrast problem and how would one go about fixing it (software or hardware)? If the problem is hardware, where would it be more probably localized? the DMD, the DLPC350 or some other place on the board?
Thank you for any help,
Bogdan
PS: The firmware is updated and the green LEDs on the board are blinking.