This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Data to be stored in the internal buffer of DLPC350

Genius 5960 points

Other Parts Discussed in Thread: DLPC350

Hi,

Please tell us about DLPC350.

I use DLPC350 in pattern sequence mode.

Data to be stored in the internal buffer of DLPC350 is,
"Bit depth the different data" Is it possible to project?

Example) 4 sheets of 8bit pattern, the 1bit pattern is 16 sheets, etc.

Best Regards,

hamada

  • Hello Hamada-san,

    Yes it is possible.

    First, you can use the GUI tool to add 4 8bit patterns + 16 1-bit patterns, for this i suggest you to a) Add three 8-bit patterns as one image in the flash b) next 1 8bit pattern + 16 1bit pattern as second image in the flash.

    Refer to User's Guide Section 3.6 Storing Images in Flash Memory section 

    Second, add the above two images in the firmware, program the firmware.

     Third, run the pattern sequence by selecting 3 8-bit patterns from the image followed by 1 8-bit and 16 1bit patterns in the next image.

    Regards,
    Sanjeev