Other Parts Discussed in Thread: DLPC350, DLP4500
Hi,
We have designed a DLP system around the DLPC350 and we seem to have an unstable image on the output. We are using the TI Flash image to program the flash memory that is connected to the DLPC350.
While the system is booting we can see the TI Splash image and its very stable and perfect in its appearance. However, when the video from our external processor (24bit RGB) is enabled, the output very is unstable and it seems to be flashing. Thus, it seems like a synchronization problem.
Upon inspection, we found that the PWM signal from the DLPC350 is unstable while video from our external controller is being displayed. When the TI Splash screen is being displayed the PWM signal is stable, hence the good video output from the DLP.
We've tried different input resolutions 800x600 @60Hz, 800x600@30Hz, 1280x800@60Hz to the DLPC350, however the problem still exists. We used the DLP4500 reference schematic (DLPC350 and the power supply sections) as a guide for our custom board.
We've studied the DLPC350 programmers manual and the datasheet and can't seem to find any information that could help us solve this problem. Is there anything you can provide us with to aid us in solving this problem?
Thanks
Glen