Hello DLP ALC team,
A parallel Flash ROM for the firmware should be connected to DLPC350.
I would like to ask you some questions about the Flash ROM. Would you please answer these questions?
Q1. What is the optimal size of this flash in case of the typical application?
There is a large size of Flash in the LightcCrafter4500 because it is used also for storing the pattern image. Thus, we would like to know what is the typical flash ROM size only for the firmware (without pattern image).
Q2. Is there any restriction of the type of parallel flash ROM for DLPC350? Or, do you have any criteria to select the flash? It looks the LightCrafter4500 is using the flash which supports a dual operation. Would you please tell us the reason why this type of flash is used?
It would be helpful if you can give any comment or advice to these questions above.
Best Regards,
Nobuyoshi Arai