Other Parts Discussed in Thread: DLPC350
As I understand it you can load images three ways. Through the RGB or FPF link interfaces. Or directly through splash screen flash memory.
And the Flash memory can be loaded directly through USB. Is that correct? We have a limited number of structured light images ( > 30) we want load and sequence out to the DMD. We are trying to understand the most efficient way to do this and minimize hardware interfaces to do it. USB directly into the chip is preferable way. We have used the 4100 DLP chipset. This seems much easier to get data into the DMD. We would prefer not to use RGB or FPD link interfaces which require more chips in front of the DLPC350.