Part Number: DLPC4422
Other Parts Discussed in Thread: DLP660TE, , DLP470NE
Hi,
I noticed in the DLPC4422 white paper that this display controller "Supports 24-30 Hz and 47-120 Hz Frame Rates". Two of these controllers need to be used in conjunction with the DLP660TE TRP DMD. My question relates to the a 24p signal being sent to a projector with this combination of hardware. I recently had an Optoma UHD65 projector which uses these display controllers with the DLP660TE TRP DMD but there seems to be 3:2 pulldown occurring with a 24p input sent to the projector. This projector forces the XPP actuator to be enabled at all times. The image is always scaled to UHD and displayed through the projector via XPR. There is no support for 1:1 pixel mapping at this DMD's native resolution. My question is; does the DLPC4422 combined with the DLP660TE TRP DMD with XPR enabled allow for 2:2 (or higher) pulldown to properly display this type of signal or is everything forced to be displayed at 60p with 3:2 pulldown being forced due to the use of XPR? I'm just curious if this is a limitation of this controller and DMD combination or if this is the fault of Optoma in how they're handling your hardware?
Any help is much appreciated!
Thanks,
Dylan