Hi, all C55 experts,
We made several hundreds equipments using TMS320C5504.
And we found 2 troubled equipments.
The sets sometimes hang up when power on.
The quality control group found this issue when power on/off tests.
When power on, C5504 boots the code from a flash memory thru SPI interface.
I/O power is 3.0V and core power is 1.3V.
DSP is working on 12MHz clock.
We already compared the object code between the flash memory and RAM, and they are just same.
SPI serial data transfer was good.
But DSP code was not executed. Main function was not executed.
Probably the content of Program Counter(PC) may be wrong.
We want to know why and when this trouble is occurred.
And of cause we want to see workaround.
We can provide any information to you if you are required.
B.R.
Massa