Tool/software: Code Composer Studio
Hi everybody!
I'm working with I2S via DMA interrupt. I'm testing the program on EZDSP5535 equipment.
When running from the CCS in the debug mode, everything works fine. The sound passes from an external source (I2S0) to a loudspeaker (I2S2) and back.
However, when I start the applicationwith with the SPI FLASH, the DMA interrupt does not occur.
Please help me solve the problem.
Aleksandr.
2555.main.c
main.h
/** * main.c */ #include "string.h" #include "main.h" //#include "ezdsp5535.h" //#include "ezdsp5535_led.h" extern void VECSTART(void); // defined in vector table CSL_IRQ_Dispatch dispatchTable; const PLL_Config pllCfg_75MHz = {0x88ED, 0x8000, 0x0806, 0x0000}; const PLL_Config pllCfg_100MHz = {0x8BE8, 0x8000, 0x0806, 0x0000}; const PLL_Config pllCfg_120MHz = {0x8E4A, 0x8000, 0x0806, 0x0000}; ProgramPLL() { PLL_Obj pllObj; PLL_Config *configInfo; PLL_Handle hPll; Uint32 pllInstId; int i; pllInstId = 0; PLL_init(&pllObj,pllInstId); hPll = &pllObj; PLL_reset(hPll); configInfo = (PLL_Config *)&pllCfg_100MHz; PLL_config(hPll, configInfo); for(i=0;i<100;i++); PLL_enable(hPll); for(i=0;i<100;i++); } #define led_green 17 #define led_red 16 #define led_yellow 15 #define led_blue 14 CSL_GpioObj GpioObj; CSL_GpioObj *hGpio; void LedInit() { int i; CSL_Status status; CSL_GpioPinConfig config; hGpio = GPIO_open(&GpioObj, &status); for(i=14; i<18; i++) { config.pinNum = i; config.direction = CSL_GPIO_DIR_OUTPUT; config.trigger = CSL_GPIO_TRIG_CLEAR_EDGE; GPIO_configBit(hGpio,&config); GPIO_write(hGpio, i, 1); } } void LedON(int number) { GPIO_write(hGpio, number, 0); } void LedOFF(int number) { GPIO_write(hGpio, number, 1); } //----------------------------------------------------------------------------- void main(void) { int i = 0; Uint32 count = 0; int on_off = 0; CSL_SYSCTRL_REGS->PCGCR1 = 0x0000; CSL_SYSCTRL_REGS->PCGCR2 = 0x0000; DeviceInit(); Uint16 signal[FRAME_LENGTH] = { 0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b, 0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef, 0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4, 0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75, 0x9128, 0x89c1, 0x845f, 0x811b, 0x8002, 0x811b, 0x845f, 0x89c1, 0x9128, 0x9a76, 0xa57f, 0xb216, 0xc002, 0xcf06, 0xdee0, 0xef4c, 0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b, 0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef, 0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4, 0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75, 0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b, 0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef, 0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4, 0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75, 0x9128, 0x89c1, 0x845f, 0x811b, 0x8002, 0x811b, 0x845f, 0x89c1, 0x9128, 0x9a76, 0xa57f, 0xb216, 0xc002, 0xcf06, 0xdee0, 0xef4c, 0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b, 0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef, 0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4, 0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75 }; while(i<5){ if(spkr_write_block(signal, signal)) i++; } while (true) { F_read_block(midl_buf_L, midl_buf_R); spkr_write_block(midl_buf_L, midl_buf_R); count++; if(count >= 50000) { if(on_off){ LedOFF(led_green); on_off = 0; } else{ LedON(led_green); on_off = 1; } count = 0; } } } //***************************************************************************** // DeviceInit //***************************************************************************** void DeviceInit() { Int16 i; Uint16 prcr; //buf clear for(i = 0; i< FRAME_LENGTH; i++) { midl_buf_L[i] = i; midl_buf_R[i] = i; } for(i = 0; i< FRAME_LENGTH*2; i++) { bufN_WL[i] = 0x0000; bufN_WR[i] = 0x0000; bufN_RL[i] = 0x0000; bufN_RR[i] = 0x0000; bufF_WL[i] = 0x0000; bufF_WR[i] = 0x0000; bufF_RL[i] = 0x0000; bufF_RR[i] = 0x0000; } IRQ_init(&dispatchTable, 0); IRQ_globalDisable(); IRQ_disableAll(); IRQ_clearAll(); Uint32 irq = (Uint32)&VECSTART; IRQ_setVecs(irq); //IRQ_clear(DMA_EVENT); // Reset all peripherals CSL_SYSCTRL_REGS->PSRCR = 0x0020; CSL_SYSCTRL_REGS->PRCR = 0x00BB; do { prcr = CSL_SYSCTRL_REGS->PRCR; } while (prcr != 0); CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_PPMODE, MODE6); CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE0); CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE1); CSL_SYSCTRL_REGS->PCGCR1 = 0x1c02; CSL_SYSCTRL_REGS->PCGCR2 = 0x0003; ProgramPLL(); LedInit(); //Init devices i2c_init(); Wait(300); DmaInit(); I2sDmaN_init(); I2sDmaF_init(); i2sN_init(); i2sF_init(); aic_init(); IRQ_globalEnable(); if(irq == 327168) LedON(led_blue); } //***************************************************************************** // DmaInit // Description: Initializes DMA, enables DMA interrupts //***************************************************************************** void DmaInit() { Uint16 ifrValue; IRQ_disable(DMA_EVENT); IRQ_clear(DMA_EVENT); IRQ_plug(DMA_EVENT, &DmaIsr); DMA_init(); IRQ_enable(DMA_EVENT); } //----------------------------------------------------------------------------- //***************************************************************************** // void i2s_init() //**************************************************************************** void i2sN_init() { CSL_I2sHandle hI2sN; I2S_Config hwConfig; /* Open the device with instance 2 */ hI2sN = I2S_open(I2S_INSTANCE2, DMA_INTERRUPT, I2S_CHAN_STEREO); /* Set the value for the configure structure */ hwConfig.dataType = I2S_STEREO_ENABLE; hwConfig.loopBackMode = I2S_LOOPBACK_DISABLE; hwConfig.fsPol = I2S_FSPOL_LOW; hwConfig.clkPol = I2S_RISING_EDGE; hwConfig.datadelay = I2S_DATADELAY_ONEBIT; hwConfig.datapack = I2S_DATAPACK_ENABLE; hwConfig.signext = I2S_SIGNEXT_DISABLE; hwConfig.wordLen = I2S_WORDLEN_16; hwConfig.i2sMode = I2S_SLAVE; hwConfig.FError = I2S_FSERROR_DISABLE; hwConfig.OuError = I2S_OUERROR_DISABLE; hwConfig.clkDiv = I2S_CLKDIV16; hwConfig.dataFormat = I2S_DATAFORMAT_DSP; hwConfig.fsDiv = I2S_FSDIV16; /* Configure hardware registers */ if(I2S_setup(hI2sN, &hwConfig) != CSL_SOK) LedON(led_blue); if(I2S_transEnable(hI2sN, TRUE) != CSL_SOK) LedON(led_blue); hI2sN->firstRead = FALSE; } //----------------------------------------------------------------------------- void i2sF_init() { CSL_I2sHandle hI2sF; I2S_Config hwConfig; /* Open the device with instance 2 */ hI2sF = I2S_open(I2S_INSTANCE0, DMA_INTERRUPT, I2S_CHAN_STEREO); /* Set the value for the configure structure */ hwConfig.dataType = I2S_STEREO_ENABLE; hwConfig.loopBackMode = I2S_LOOPBACK_DISABLE; hwConfig.fsPol = I2S_FSPOL_LOW; hwConfig.clkPol = I2S_RISING_EDGE; hwConfig.datadelay = I2S_DATADELAY_ONEBIT; hwConfig.datapack = I2S_DATAPACK_ENABLE; hwConfig.signext = I2S_SIGNEXT_DISABLE; hwConfig.wordLen = I2S_WORDLEN_16; hwConfig.i2sMode = I2S_SLAVE; hwConfig.FError = I2S_FSERROR_DISABLE; hwConfig.OuError = I2S_OUERROR_DISABLE; hwConfig.clkDiv = I2S_CLKDIV16; hwConfig.dataFormat = I2S_DATAFORMAT_DSP; hwConfig.fsDiv = I2S_FSDIV16; /* Configure hardware registers */ if(I2S_setup(hI2sF, &hwConfig) != CSL_SOK) LedON(led_blue); if(I2S_transEnable(hI2sF, TRUE) != CSL_SOK) LedON(led_blue); hI2sF->firstRead = FALSE; } //***************************************************************************** // I2sDmaInit // Configures and starts I2S with DMA //***************************************************************************** void I2sDmaN_init() { CSL_DMA_Config dmaConfig; CSL_Status status; // Configure DMA ch4 for I2S left write (�� �������) dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S2_TX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_WRITE; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH_10*4; // two frames dmaConfig.srcAddr = (Uint32)bufN_WLPi; dmaConfig.destAddr = (Uint32)&CSL_I2S2_REGS->I2STXLT0; dmaNLeftTxHandle = DMA_open(DMA_N_CHAN_TX_L, &dmaObj0,&status); if(DMA_config(dmaNLeftTxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaNLeftTxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch5 for I2S right write (�� �������) dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S2_TX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_WRITE; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH_10*4; // two frames dmaConfig.srcAddr = (Uint32)bufN_WRPi; dmaConfig.destAddr = (Uint32)&CSL_I2S2_REGS->I2STXRT0; dmaNRightTxHandle = DMA_open(DMA_N_CHAN_TX_R, &dmaObj1,&status); if(DMA_config(dmaNRightTxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaNRightTxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch6 for I2S left read (�� ���������) dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S2_RX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_READ; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)&CSL_I2S2_REGS->I2SRXLT0; dmaConfig.destAddr = (Uint32)bufN_RLPi; dmaNLeftRxHandle = DMA_open(DMA_N_CHAN_RX_L, &dmaObj2,&status); if(DMA_config(dmaNLeftRxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaNLeftRxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch7 for I2S right read (�� ���������) dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S2_RX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_READ; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)&CSL_I2S2_REGS->I2SRXRT0; dmaConfig.destAddr = (Uint32)bufN_RRPi; dmaNRightRxHandle = DMA_open(DMA_N_CHAN_RX_R, &dmaObj3,&status); if(DMA_config(dmaNRightRxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaNRightRxHandle) != CSL_SOK) LedON(led_blue); flagN_RI = 0; flagN_WI = 0; } //------------------------------------------------------------------ void I2sDmaF_init() { CSL_DMA_Config dmaConfig; CSL_Status status; // Configure DMA ch0 for I2S left write dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S0_TX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_WRITE; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)bufF_WLPi; dmaConfig.destAddr = (Uint32)&CSL_I2S0_REGS->I2STXLT0; dmaFLeftTxHandle = DMA_open(DMA_F_CHAN_TX_L, &dmaObj4,&status); if(DMA_config(dmaFLeftTxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaFLeftTxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch1 for I2S right write dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S0_TX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_WRITE; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)bufF_WRPi; dmaConfig.destAddr = (Uint32)&CSL_I2S0_REGS->I2STXRT0; dmaFRightTxHandle = DMA_open(DMA_F_CHAN_TX_R, &dmaObj5,&status); if(DMA_config(dmaFRightTxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaFRightTxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch2 for I2S left read dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S0_RX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_READ; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)&CSL_I2S0_REGS->I2SRXLT0; dmaConfig.destAddr = (Uint32)bufF_RLPi; dmaFLeftRxHandle = DMA_open(DMA_F_CHAN_RX_L, &dmaObj6,&status); if(DMA_config(dmaFLeftRxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaFLeftRxHandle) != CSL_SOK) LedON(led_blue); // Configure DMA ch3 for I2S right read dmaConfig.pingPongMode = CSL_DMA_PING_PONG_ENABLE; dmaConfig.autoMode = CSL_DMA_AUTORELOAD_ENABLE; dmaConfig.burstLen = CSL_DMA_TXBURST_2WORD; dmaConfig.trigger = CSL_DMA_EVENT_TRIGGER; dmaConfig.dmaEvt = CSL_DMA_EVT_I2S0_RX; dmaConfig.dmaInt = CSL_DMA_INTERRUPT_ENABLE; dmaConfig.chanDir = CSL_DMA_READ; dmaConfig.trfType = CSL_DMA_TRANSFER_IO_MEMORY; dmaConfig.dataLen = FRAME_LENGTH*4; // two frames dmaConfig.srcAddr = (Uint32)&CSL_I2S0_REGS->I2SRXRT0; dmaConfig.destAddr = (Uint32)bufF_RRPi; dmaFRightRxHandle = DMA_open(DMA_F_CHAN_RX_R, &dmaObj7,&status); if(DMA_config(dmaFRightRxHandle, &dmaConfig) != CSL_SOK) LedON(led_blue); if(DMA_start (dmaFRightRxHandle) != CSL_SOK) LedON(led_blue); flagF_RI = 0; flagF_WI = 0; } //------------------------------------------------------------------ //***************************************************************** // Iterupt DMA //***************************************************************** interrupt void DmaIsr(void) { CSL_Status status; volatile Uint16 ifrValue; // Clear the DMA interrupt ifrValue = CSL_SYSCTRL_REGS->DMAIFR; CSL_SYSCTRL_REGS->DMAIFR |= ifrValue; //Ch 4, 5 Write to SPKR if (ifrValue & (1<<4)){ flagN_WI = 1; if(DMA_getLastTransferType (dmaNLeftTxHandle, &status)){ flagN_WLPP = 0; } else{ flagN_WLPP = 1; } } if (ifrValue & (1<<5)){ flagN_WI = 1; if(DMA_getLastTransferType (dmaNRightTxHandle, &status)){ flagN_WRPP = 0; } else{ flagN_WRPP = 1; } } //Ch 6, 7 Read from MIC if (ifrValue & (1<<6)){ flagN_RI = 1; if(DMA_getLastTransferType (dmaNLeftRxHandle, &status)){ flagN_RLPP = 0; } else{ flagN_RLPP = 1; } } if (ifrValue & (1<<7)){ flagN_RI = 1; if(DMA_getLastTransferType (dmaNRightRxHandle, &status)){ flagN_RRPP = 0; } else{ flagN_RRPP = 1; } } //Ch 0, 1 Write to ������� ����� if (ifrValue & (1<<0)){ flagF_WI = 1; if(DMA_getLastTransferType (dmaFLeftTxHandle, &status)){ flagF_WLPP = 0; } else{ flagF_WLPP = 1; } } if (ifrValue & (1<<1)){ flagF_WI = 1; if(DMA_getLastTransferType (dmaFRightTxHandle, &status)){ flagF_WRPP = 0; } else{ flagF_WRPP = 1; } } //Ch 2, 3 Read from ������� ����� if (ifrValue & (1<<2)){ flagF_RI = 1; if(DMA_getLastTransferType (dmaFLeftRxHandle, &status)){ flagF_RLPP = 0; } else{ flagF_RLPP = 1; } } if (ifrValue & (1<<3)){ flagF_RI = 1; if(DMA_getLastTransferType (dmaFRightRxHandle, &status)){ flagF_RRPP = 0; } else{ flagF_RRPP = 1; } } } //------------------------------------------------------------------------------- void mic_read_block(Uint16* buffer_left, Uint16* buffer_right) { int i; Uint32* bL = (Uint32*)buffer_left; Uint32* bR = (Uint32*)buffer_right; Uint32* dmaL; Uint32* dmaR; while(flagN_RI == 0); flagN_RI = 0; if(flagN_RLPP == 1){ dmaL = (Uint32*)(&bufN_RL[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *bL++ = *dmaL++; } else{ dmaL = (Uint32*)(&bufN_RL[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *bL++ = *dmaL++; } if(flagN_RRPP == 1){ dmaR = (Uint32*)(&bufN_RR[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *bR++ = *dmaR++; } else{ dmaR = (Uint32*)(&bufN_RR[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *bR++ = *dmaR++; } } //------------------------------------------------------------------ volatile int f1=0; int c1=0; int spkr_write_block(Uint16* buffer_left, Uint16* buffer_right) { int i; Uint32* bL = (Uint32*)buffer_left; Uint32* bR = (Uint32*)buffer_right; Uint32* dmaL; Uint32* dmaR; if(flagN_WI == 1) flagN_WI = 0; else return 0; if(flagN_WLPP == 1){ dmaL = (Uint32*)(&bufN_WL[0]); for (i = 0; i < FRAME_LENGTH_10/2; i++) *dmaL++ = *bL++; } else { dmaL = (Uint32*)(&bufN_WL[FRAME_LENGTH_10]); for (i = 0; i < FRAME_LENGTH_10/2; i++) *dmaL++ = *bL++; } if(flagN_WRPP == 1){ dmaR = (Uint32*)(&bufN_WR[0]); for (i = 0; i < FRAME_LENGTH_10/2; i++) *dmaR++ = *bR++; } else{ dmaR = (Uint32*)(&bufN_WR[FRAME_LENGTH_10]); for (i = 0; i < FRAME_LENGTH_10/2; i++) *dmaR++ = *bR++; } c1++; if(c1 >= 100) { if(f1){ LedON(led_yellow); f1 = 0; } else{ LedOFF(led_yellow); f1 = 1; } c1 = 0; } return 1; } //------------------------------------------------------------------------- volatile int f=0; int co=0; void F_read_block(Uint16* buffer_left, Uint16* buffer_right) { int i; Uint32* bL = (Uint32*)buffer_left; Uint32* bR = (Uint32*)buffer_right; Uint32* dmaL; Uint32* dmaR; if(flagF_RI == 1) flagF_RI = 0; else return; if(flagF_RLPP == 1){ dmaL = (Uint32*)(&bufF_RL[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *bL++ = *dmaL++; } else{ dmaL = (Uint32*)(&bufF_RL[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *bL++ = *dmaL++; } if(flagF_RRPP == 1){ dmaR = (Uint32*)(&bufF_RR[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *bR++ = *dmaR++; } else{ dmaR = (Uint32*)(&bufF_RR[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *bR++ = *dmaR++; } co++; if(co>100){ if(f==0){ LedON(led_red); f=1; } else{ LedOFF(led_red); f=0; } co=0; } } //------------------------------------------------------------------ void F_write_block(Uint16* buffer_left, Uint16* buffer_right) { int i; Uint32* bL = (Uint32*)buffer_left; Uint32* bR = (Uint32*)buffer_right; Uint32* dmaL; Uint32* dmaR; while(flagF_WI == 0); flagF_WI = 0; if(flagF_WLPP == 1){ dmaL = (Uint32*)(&bufF_WL[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *dmaL++ = *bL++; } else { dmaL = (Uint32*)(&bufF_WL[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *dmaL++ = *bL++; } if(flagF_WRPP == 1){ dmaR = (Uint32*)(&bufF_WR[0]); for (i = 0; i < FRAME_LENGTH/2; i++) *dmaR++ = *bR++; } else{ dmaR = (Uint32*)(&bufF_WR[FRAME_LENGTH]); for (i = 0; i < FRAME_LENGTH/2; i++) *dmaR++ = *bR++; } } //------------------------------------------------------------------------- //************************************************************************* //I2C Init //************************************************************************* void i2c_init() { volatile Uint16 looper; volatile Uint32 csl_i2c_sys_clk; /* Initialize I2C module */ I2C_init(CSL_I2C0); csl_i2c_sys_clk = GetSysClk(); /* Setup I2C module */ i2cSetup.addrMode = CSL_I2C_ADDR_7BIT; i2cSetup.bitCount = CSL_I2C_BC_8BITS; i2cSetup.loopBack = CSL_I2C_LOOPBACK_DISABLE; i2cSetup.freeMode = CSL_I2C_FREEMODE_DISABLE; i2cSetup.repeatMode = CSL_I2C_REPEATMODE_DISABLE; i2cSetup.ownAddr = CSL_I2C_OWN_ADDR; //sysclk to i2c, before pre-scaling i2cSetup.sysInputClk = csl_i2c_sys_clk/1000u; //actual i2c serial clk i2cSetup.i2cBusFreq = CSL_I2C_BUS_FREQ; startStop = ((CSL_I2C_START) | (CSL_I2C_STOP)); I2C_setup(&i2cSetup); } //----------------------------------------------------------------- Uint32 GetSysClk() { Bool pllRDBypass; Bool pllOutDiv; Uint32 sysClk; Uint16 pllM; Uint16 pllRD; Uint16 pllOD; pllM = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR1, SYS_CGCR1_M); pllRD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDRATIO); pllOD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_ODRATIO); pllRDBypass = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDBYPASS); pllOutDiv = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_OUTDIVEN); sysClk = 32768u;//CSL_PLL_CLOCKIN; if (0 == pllRDBypass) { sysClk = sysClk/(pllRD + 4); } sysClk = (sysClk * (pllM + 4)); if (1 == pllOutDiv) { sysClk = sysClk/(pllOD + 1); } /* Return the value of system clock in KHz */ return(sysClk/1000); } //------------------------------------------------------------------------- //************************************************************************* // AIC Init //************************************************************************ Int16 AIC3204_rget( Uint16 regnum, Uint16* regval ) { Int16 retcode = 0; Uint16 cmd[2]; cmd[0] = regnum & 0x007F; // 7-bit Device Register cmd[1] = 0; Uint16 startStop = ((CSL_I2C_START) | (CSL_I2C_STOP)); I2C_write(cmd, 2, AIC3204_I2C_ADDR, TRUE, startStop, CSL_I2C_MAX_TIMEOUT); //I2C_read(cmd, 1, AIC3204_I2C_ADDR, NULL, 0. TRUE, startStop, // CSL_I2C_MAX_TIMEOUT, FALSE); *regval = cmd[0]; Wait_tact( 10 ); return retcode; } //-------------------------------------------------------------------------- void AIC3204_rset( Uint16 regnum, Uint16 regval ) { Uint16 cmd[2]; cmd[0] = (regnum & 0x00FF); // 7-bit Device Register cmd[1] = (regval & 0x00FF); // 8-bit Register Data Wait(300); Uint16 startStop = ((CSL_I2C_START) | (CSL_I2C_STOP)); I2C_write(cmd, 2, AIC3204_I2C_ADDR, TRUE, startStop, CSL_I2C_MAX_TIMEOUT); } //**************************************************************************** //AIC init //**************************************************************************** void aic_init() { // Configure AIC3204 AIC3204_rset( 0, 0x00 ); // Select page 0 AIC3204_rset( 1, 0x01 ); // Reset codec Wait(1000); // Wait 1ms after reset AIC3204_rset( 0, 0x01 ); // Select page 1 AIC3204_rset( 1, 0x08 ); // Disable crude AVDD generation from DVDD AIC3204_rset( 2, 0x01 ); // Enable Analog Blocks, use LDO power AIC3204_rset( 123,0x05 ); // Force reference to power up in 40ms Wait(50000); // Wait at least 40ms AIC3204_rset( 0, 0x00 ); // Select page 0 // PLL and Clocks config and Power Up if(AIC_SAMPLE_SIZE == 32) AIC3204_rset( 27, 0x3d ); // BCLK and WCLK are set as o/p; AIC3204(Master); 32-bit sample else AIC3204_rset( 27, 0x0d ); // BCLK and WCLK are set as o/p; AIC3204(Master); 16-bit sample AIC3204_rset( 28, 0x00 ); // Data ofset = 0 AIC3204_rset( 4, 0x03 ); // PLL setting: PLLCLK <- MCLK, CODEC_CLKIN <-PLL CLK AIC3204_rset( 6, 0x07 ); // PLL setting: J=7 AIC3204_rset( 7, 0x06 ); // PLL setting: HI_BYTE(D=1680) AIC3204_rset( 8, 0x90 ); // PLL setting: LO_BYTE(D=1680) AIC3204_rset( 30, 0x88 ); // For 32 bit clocks per frame in Master mode ONLY // BCLK=DAC_CLK/N =(12288000/8) = 1.536MHz = 32*fs AIC3204_rset( 5, 0x91 ); // PLL setting: Power up PLL, P=1 and R=1 Wait(10000); // Wait for PLL to come up AIC3204_rset( 13, 0x00 ); // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling AIC3204_rset( 14, 0x80 ); // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080 AIC3204_rset( 20, 0x80 ); // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6 AIC3204_rset( 11, 0x82 ); // Power up NDAC and set NDAC value to 2 AIC3204_rset( 12, 0x95 ); // Power up MDAC and set MDAC value to 7 AIC3204_rset( 18, 0x95 ); // Power up NADC and set NADC value to 7 AIC3204_rset( 19, 0x82 ); // Power up MADC and set MADC value to 2 // DAC ROUTING and Power Up AIC3204_rset( 0, 0x01 ); // Select page 1 AIC3204_rset( 12, 0x08 ); // LDAC AFIR routed to HPL AIC3204_rset( 13, 0x08 ); // RDAC AFIR routed to HPR AIC3204_rset( 0, 0x00 ); // Select page 0 AIC3204_rset( 64, 0x02 ); // Left vol=right vol AIC3204_rset( 65, 0x00 ); // Left DAC gain to 0dB VOL; Right tracks Left AIC3204_rset( 63, 0xd4 ); // Power up left,right data paths and set channel AIC3204_rset( 0, 0x01 ); // Select page 1 AIC3204_rset( 16, 0x00 ); // Unmute HPL , 0dB gain AIC3204_rset( 17, 0x00 ); // Unmute HPR , 0dB gain AIC3204_rset( 9 , 0x30 ); // Power up HPL,HPR Wait(100 ); // Wait // ADC ROUTING and Power Up AIC3204_rset( 0, 0x01 ); // Select page 1 AIC3204_rset( 51, 0x48); // power up MICBIAS with AVDD (0x40)or LDOIN (0x48) //MM - added micbias AIC3204_rset( 52, 0x30 ); // STEREO 1 Jack // IN2_L to LADC_P through 40 kohm AIC3204_rset( 55, 0x30 ); // IN2_R to RADC_P through 40 kohmm AIC3204_rset( 54, 0x03 ); // CM_1 (common mode) to LADC_M through 40 kohm AIC3204_rset( 57, 0xc0 ); // CM_1 (common mode) to RADC_M through 40 kohm AIC3204_rset( 59, 60 ); // MIC_PGA_L unmute AIC3204_rset( 60, 60 ); // MIC_PGA_R unmute AIC3204_rset( 0, 0x00 ); // Select page 0 AIC3204_rset( 81, 0xc0 ); // Powerup Left and Right ADC AIC3204_rset( 82, 0x00 ); // Unmute Left and Right ADC AIC3204_rset( 0, 0x00 ); // Select page 0 Wait(100 ); // Wait }