As I asked before
Can I update FW (Image) or data (file system) with the program UniFlash of a CC3100mod on my board?
Is it enough to power the module and with pin HIB (4) and Pin nReset (35) to bring CC100mod in Boot mode
and, after thet, to connect it with Uniflash via UART (pin 46 - pin 47) andwith a cable type FTDI convert
USB 232R - 3.3 V logic?
Is it so?
Or have I to use the CC31XXEMUBOOST interface?