Other Parts Discussed in Thread: WL1831
Hi All,
We are using wl1831 module from TI in our custom board with imx6 processor.
We need to implement the A2DP sink profile. Mobile device will play audio and it should be listenable on board speaker through bluetooth.
We are using Bluez4 with Pulseaudio 5.0 and SBC 1.2.
The problem with our setup is , Mobile device is not getting detected as bluez source.
Below are the changes i have done to implement Bluetooth A2DP sink profile
- /etc/bluetooth/audio.conf
Enable=Source,Sink,Media,Socket
SBCSources=1
- /etc/dbus-1/system.d/bluetooth.conf
<busconfig>
<!-- ../system.conf have denied everything, so we just punch some holes -->
<policy context="default">
<allow own="org.bluez"/>
<allow send_destination="org.bluez"/>
<allow send_interface="org.bluez.Agent"/>
</policy>
<!-- allow users at the console, see consolekit or libpam-foreground -->
<policy at_console="true">
<allow send_destination="org.bluez"/>
</policy>
<policy user="pulse">
<allow send_destination="org.bluez"/>
<allow send_interface="org.freedesktop.DBus.ObjectManager"/>
</policy>
</busconfig>
- /etc/dbus-1/system.d/pulseaudio-system.conf
<busconfig>
<!-- System-wide PulseAudio runs as 'pulse' user. This fragment is
not necessary for user PulseAudio instances. -->
<policy user="pulse">
<allow own="org.pulseaudio.Server"/>
<allow send_destination="org.bluez"/>
<allow send_interface="org.freedesktop.DBus.ObjectManager"/>
</policy>
</busconfig>
- /etc/pulse/system.pa
.ifexists module-bluetooth-policy.so
load-module module-bluetooth-policy
.endif
.ifexists module-bluetooth-discover.so
load-module module-bluetooth-discover
.endif
load-module module-switch-on-connect
- /etc/pulse/daemon.conf
; resample-method = trivial
============================================================
Procedure after boot:
hciconfig hci0 up
bluetooth -n &
hciconfig hci0 piscan
pulseaudio --system --realtime &
hcitool scan
bt-device -c <BD-Address>
Here i am getting this log.
E: [pulseaudio] bluez4-util.c: org.bluez.HandsfreeGateway.GetProperties() failed: org.freedesktop.DBus.Error.Unknowt
E: [pulseaudio] bluez4-util.c: org.bluez.HandsfreeGateway.GetProperties() failed: org.freedesktop.DBus.Error.UnknownMethod: Method "Get
and when i run,
pactl load-module module-bluez4-device path=<path> name=<name> address=<BD-Address>
I am getting,
W: [pulseaudio] module-bluez4-device.c: Profile 'a2dp' not valid or not supported by device.
W: [pulseaudio] module-bluez4-device.c: Default profile not connected, selecting off profile
but if i do sdptool browse <BD-address>, I am seeing that device supports the a2dp.
Now, if i see the sources with "pactl list sources short", It does not show the bluez source for my paired mobile.
=========================================================================================
Questions:
- Do i need to do anything special for TI specific module?
- Do TI modules supports a2dp sink profile with Bluez4 stack?
- Is it anything related to Bluetooth firmware? To and From data transfer is fine.
Please provide your suggestions
Thanks,
Jags