Hi,
My customer is using Hyperlink in between two C6678s and now having the issue on HYPERLINK_SERDES_STS register. It indicates EQOVER=1 and EQUNDER=1 with Fully adaptive equalization enabled. First of all, is this fatal error for correct behavior of Hyperlink ? For example, with this state, is there any possibility to get wrong data via Hyperlink ?
They are watching the following post and also they are reading the keystone serdes user guide. In order to optimize the EQ level, they are trying to control TWPRE and TWPST1 on HYPERLINK_SERDES_CFGTXn registers, but they could not reach to the condition of EQOVER=0 and EQUNDER=0. It seems the link itself is ok, but they has not been able to read the remote Hyperlink configuration registers. We want to know if this EQ errors are critical for the issue.
Best Regards,
Naoki Kawada