Hi all,
I am facing bad data CRC error issue frequently after write the kernel uImage into NAND,
if i kept my dm355 evm board for 10 to 15 days in switch OFF condition then my board getting into this issue.
Information about hardware:
-------------------------------------------
=====
LOG
=====
Chip initialization passed!
TI UBL Version: 1.30
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid MagicNum found.
ENTRY POINT = 0x81080000
NUM PAGES = 0x00000050
BLOCK = 0x00000019
PAGE = 0x00000001
LOAD ADDRESS = 0x81080000 DONE
Jumping to entry point at 0x81080000.
LSP 2.10 BETA RELEASE
VERSION: 2.10.008.02
U-Boot 1.3.4 (Jul 26 2010 - 11:34:57)
I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit)
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
No NAND device found!!!
512 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 216MHz
DDR Clock :- 171MHz
Hit any key to stop autoboot: 4 3 2 1 0
Loading from NAND 512MiB 3,3V 8-bit, offset 0x400000
Image Name: Linux-2.6.18-lsp2.10_hw2.1_withE
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1700372 Bytes = 1.6 MB
Load Address: 80008000
Entry Point: 80008000
** Read error
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18-lsp2.10_hw2.1_withE
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1700372 Bytes = 1.6 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
DM355 EVM :>
Thanks & Regards,
S.Titus.