Hello,
My basic usecase is to stream the video on a computer using VLC media player. I do not want any noise filter for now. I could also use a basic VGA camera to interface and stream the video. I have the following questions:
1. How to make the demo work in Low Power mode. The demo works fine in Full Feature Mode. I get the following errors when the demo is run on low power mode.
[ 20.891501] autorun-usecase.sh[114]: ApproDrvInit: 7 [ 20.893185] autorun-usecase.sh[114]: queue id:163845 [ 26.961326] autorun-usecase.sh[114]: queue id:0 [ 29.067306] autorun-usecase.sh[114]: ApproDrvInit: 3 [ 29.079647] autorun-usecase.sh[114]: queue id:163845 [ 30.980622] autorun-usecase.sh[114]: queue id:0 [ 46.964384] autorun-usecase.sh[114]: TimeOut occure in boot_proc. [ 46.965145] autorun-usecase.sh[114]: Program exit.
2. If I want a resolution of 640x480, does the given application software support this configuration.