This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/DM3730: After installing DVSDK iso image it's not showing BIN folder? How to create SD card without mksdboot.sh file?

Part Number: DM3730

Tool/software: Linux

Hi

i am downloaded latest versionof DVSDK v4.03.00.06 version in ubuntu and installed, But BIN Folder & mksdboot.sh file not created how can i Run mksdboot script installed in DVSDK as show below

sudo ${DVSDK}/bin/mksdboot.sh --device /dev/sdc --sdk ${DVSDK}-------------------------->(No path it's showing it means NO files),

i am installed in ubuntu 10.04 LTS OS.

Thank you

Regards,

ram.

  • Hi Ram,

    Please provide the below console output for analysis:

    host$ uname -a
    host$ ./dvsdk_dm3730-evm_04_03_00_06_setuplinux

    Regards,
    Pavel



  • In reply to Pavel Botev:

    Hi pavel,

    i am attached the suggestion commands please check and give the things

    regards,

    ram

  • In reply to Ramachandra Parlapalli:

    Ram,

    Click on the "yes" button, and provide the next part of the log, till the successful SDK installation.



  • In reply to Pavel Botev:

    hi Pavel,

    I have taken print screens some pics are there below

  • In reply to Ramachandra Parlapalli:

  • In reply to Ramachandra Parlapalli:

    Ram,

    Please provide the output of the below command:

    host $ls -al /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06

    Regards,
    Pavel



  • In reply to Pavel Botev:

    Pavel,
    Sorry for the disturbance that particular DVSDK-4.03 not fully installed or corrupted, once again i downloaded and installed the DVSDK-4.03 version it is working and generating bin file,
    But in this case also gcc not found showing.
    1.How to build native gcc or any gcc bin file wecan add in rootfs/bin/gcc it will works.
    2.where to build native gcc compiler(Linaro)
    could you give me some suggestions
    Thanking you,
    Regards,
    Ram
  • In reply to Ramachandra Parlapalli:

    Ram,

    DM37x SDK support only GCC cross compiler. It is available at SDK/linux-devkit/ folder.

    Native compiler and cross compiler are discussed (suggestions already provided) in the below e2e thread, nothing more to add.

    https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/537/t/653251



    Regards,
    Pavel



This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.