Hi,
I am having a problem when building the TI81XX-LINUX-PSP-04.04.00.02/src/kernel/linux-04.04.00.02 kernel (uImage in particular).
Towards the End, I am getting the following errors:
LD arch/arm/boot/compressed/vmlinux
arm-none-linux-gnueabi-ld: error: arch/arm/boot/compressed/piggy.gzip.o: Unknown CPU architecture
arm-none-linux-gnueabi-ld: error: arch/arm/boot/compressed/lib1funcs.o: Unknown CPU architecture
I am building using the following command:
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm uImage
And, yes, I am using linux Cross-compiling tools that are obtained from Gentoo/Debian, not the arago tools.
Can anyone tell me what I need to fix on these files for the system to know what the CPU architecture is?
My tools are:Using built-in specs.
COLLECT_GCC=/usr/i686-pc-linux-gnu/arm-none-linux-gnueabi/gcc-bin/4.8.1/arm-none-linux-gnueabi-gcc
COLLECT_LTO_WRAPPER=/usr/libexec/gcc/arm-none-linux-gnueabi/4.8.1/lto-wrapper
Target: arm-none-linux-gnueabi
Configured with: /var/tmp/portage/cross-arm-none-linux-gnueabi/gcc-4.8.1-r1/work/gcc-4.8.1/configure --prefix=/usr --bindir=/usr/i686-pc-linux-gnu/arm-none-linux-gnueabi/gcc-bin/4.8.1 --includedir=/usr/lib/gcc/arm-none-linux-gnueabi/4.8.1/include --datadir=/usr/share/gcc-data/arm-none-linux-gnueabi/4.8.1 --mandir=/usr/share/gcc-data/arm-none-linux-gnueabi/4.8.1/man --infodir=/usr/share/gcc-data/arm-none-linux-gnueabi/4.8.1/info --with-gxx-include-dir=/usr/lib/gcc/arm-none-linux-gnueabi/4.8.1/include/g++-v4 --host=i686-pc-linux-gnu --target=arm-none-linux-gnueabi --build=i686-pc-linux-gnu --disable-altivec --disable-fixed-point --without-cloog --disable-lto --enable-nls --without-included-gettext --with-system-zlib --enable-obsolete --disable-werror --enable-secureplt --disable-multilib --disable-libmudflap --disable-libssp --enable-libgomp --with-python-dir=/share/gcc-data/arm-none-linux-gnueabi/4.8.1/python --enable-poison-system-directories --enable-checking=release --disable-libgcj --enable-libstdcxx-time --enable-languages=c,c++,fortran --with-sysroot=/usr/arm-none-linux-gnueabi --disable-bootstrap --enable-__cxa_atexit --enable-clocale=gnu --with-bugurl=http://bugs.gentoo.org/ --with-pkgversion='Gentoo 4.8.1-r1 p1.2, pie-0.5.7'
Thread model: posix
gcc version 4.8.1 (Gentoo 4.8.1-r1 p1.2, pie-0.5.7)
and
#arm-none-linux-gnueabi-ld --version
GNU ld (GNU Binutils) 2.22.90.20120727
Copyright 2012 Free Software Foundation, Inc.
This program is free software; you may redistribute it under the terms of
the GNU General Public License version 3 or (at your option) a later version.
This program has absolutely no warranty.
Sorry if this is a dumb question.
Thanks,