Hi,
Our customer would like to use TPS62140 (or TPS62140A) on the following condition.
Could you please give us your advice.
<Condition>
・PVIN = 2.7V to 4.2V
・AVIN = 3.1V
・Vout = 1.1V
・Iout = 1.0A
<Questions>
・Shouldn’t we separate PVIN from AVIN?
・If we can separate PVIN from AVIN, Can I input 2.7V to 4.2V to PVIN?
And , Is there the limitation of the input sequence?