Other Parts Discussed in Thread: CC2540,
Hi All, Fredric,
We looked at the document. We need to look at it further but it looks like it is outlining what you would need to do from the FCC point of view and injecting a signal that is supposed to interfere with the BLE. It involved sending 1500 packets and then seeing which ones were corrupt, with a certain percentage ok being a good test and bad if percentage was below that level. I didn't see any reference to FW or routines, etc, as to, for example, sending the 1500 packets. It also had frequencies/channels. The test seemed to involved being on the lowest and highest channels (2402mHz and 2480mHz). So it looks like you would be running the modem test, but not sure how you would send out 1500 packets. I know the other MCU we use which is the TI CC2540 does have specific data patterns you can send out on the transmit test. But it doesn't look like the CC2650 has that capability. Any additional clues on how to send out 1500 packets to do the test?
Thanks,
Harold (senior sftwr lead) / Bill
Mirion Technologies Inc.