Whilst using the SM470 processor we have seen two unusual phenomenon relating to the processor reset line RSTn.
Firstly, the external pull up required to ensure the processor comes out of reset at power up is incredibly small at 10 ohms. Values as tiny as 100 ohms still prevent the unit reliably exiting reset on power up. However, this working and has been for some time.
Presently however, a futher reset problem has now occurred. When programming the unit via JTAG, Keil returns a warning "Could not stop ARM device. Please check JTAG cable".
Externally at the RSTn pin the voltage measured appears consistent with a working board. No modifications have been made to the hardware. The JTAG interface is working as I can retrieve the chip ID in the debugger.
Do you have any suggestions where to start looking for clues as to what is going wrong please.
Kindes thanks
Andrew