Help confirm whether the following settings to meet DM8168,
1.The model number is TMS320DM8168CCYG2
2.The maximum minimum range of AVS is
0.89V~1.07V,AVS Set the step range 0.02V,And Is the AVS constantly adjusting?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
0.89V~1.07V
0.89V~1.07V,AVS Set the step range 0.02V,