Hello
When the CCS3.3 starts It outputs error window which has "Cannot load DSP device driver C:\CCStudio_v3.3\drivers\tixds560icepick_c.dvr. Please
run the Setup Program and select a different driver".
I installed "setup_DM6467_CSP_v3.3.1008.exe" from TI update site and have selected "DM6467 XDS560 Emulator" in CCS setup program .
I'm using XDS560R emulator made by the Spectrumdigital.
System configuration structure which is located most left pannel of CCS setup is below.
DM6467_xds560 ->
ICEPICK_C_0 ->
Subpath_0->
ARM926_0
Subpath_1->
C6400PLUS_0
Subpath_2->
ARM968_0
Subpath_3->
ARM968_1
thanks.