Hi
The error below occasionally happens but unfortunately it is getting so frequent that I've got to find out why. From a power on reset, the target runs OK. But after I break, run the same GEL that I run on Connect, and then reload the target, I get the errors below.
Any idea[*I] what I should look at to find out what is causing this annoying problem?
Thx
Using CCS 3.3.82.
******CCS popup window************************
Can't Run Target CPU:
Error 0x00000024/-1060
Error during: Register, Execution,
An unknown error prevented the emulator from accessing the processor
in a timely fashion.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
******CCS output window*************************
Can't Run Target CPU: Error 0x00000024/-1060 Error during: Register, Execution, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.
Can't Run Target CPU: Error 0x00000024/-1060 Error during: Register, Execution, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.