Hi,
I have an application that was developed to run on the L-138 SDK . I have ported the application to run on the C6748 LCDK. I can load and run the application from the debugger but cannot run from flash. Was wondering if there is some obvious reason why the application will not run from flash. I noticed that the sysbios demos available are running on version 6.33.1.25(6.35.4.50). Does the C6748 LCDK support previous versions of sysbios? Currently running on version 5x. I reduced main to a while(1) loop and the code never gets there. Appears that the application is never being called. Any way to verify what is executing and what is actually running? If I connect the debugger the addresses present are not in the memory map. Any suggestions or help would be appreciated.
Steve