Hello everyone,
Apologies in advance if this is noddy question, or if this is in the wrong forum.
I have successfully installed the ez430-Chronos development environment on my win7 machine and have written a little C++ program that records the watch's orientation. I need to port this software over to a Raspberry Pi.
I have created a fresh Raspbian install (Raspberry Pi version of Debian wheezy), which boots up fine, but I cannot install the ez430-chronos Control Center, which I need to provide me with the libraries / drivers for my C++ project.
I have installed the required packages
apt-get install tcl8.5
apt-get install tk8.5
apt-get install xdotool
I have downloaded the latest ez430 linux software from the Ti site
root@raspberrypi:~# wget www.ti.com/lit/zip/slac388
unzipped slac388 to obtain the Chronos-Setup file
root@raspberrypi:~# unzip slac388
Made Chronos-Setup executable
root@raspberrypi:~# chmod +x Chronos-Setup
and here is where I get stuck- running the file
root@raspberrypi:~# ./Chronos-Setup
-bash: ./Chronos-Setup: cannot execute binary file
Which does not work, and produces the above error.
I cannot find anyone that seems to be having the same issue. I have followed several tutorials,
http://www.designspark.com/blog/using-the-ez430-chronos-with-a-raspberry-pi
and the slau292d.pdf ez430 user manual section 2.2.2 Linux® Installation
all to no avail. Can anyone offer any suggestions? Have I done something really daft?
Kind regards,
Richard