I am working on DM365 custom board (kernel version is 2.6.32.17-davinci1). The ov5642 sensor is connected to board and camera is up and running i.e., could able to store the video raw data file to SD card. Now, I want to convert the raw data into mpeg4 format.
I am using dvsdk encode application (dvsdk_3_10_00_19) to capture and store in mpeg4 file format. I could able to load the modules (cmemk, irqk, edmak and dm365mmap) succuessfully using loadmodules.sh. If I try to run the encode demo, it displays error message "Error: Failed to detect video standard, video input connected?"
The bootargs is
setenv bootargs console=ttyS0,115200n8 rw noinitrd ip=192.168.100.2 root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock mem
=60M video=davincifb:vid0=OFF:vid1=OFF:osd0=1280x720x16,4050K
dm365_imp.oper_mode=0 vpfe_capture.interface=1
davinci_capture.device_type=3 davinci_enc_mngr.ch0_output=COMPOSITE
davinci_enc_mngr.ch0_mode=ntsc
Parameters passed to encode allication is
root@dm365-evm:~/Test# ./encode -v ng.mpeg4 -y 1
Encode demo started.
Error: Failed to detect video standard, video input connected?
root@dm365-evm:~/Test#
Please let me know pointers/suggestions to fix this.
Thanks in Advance......