This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugger-Faild on LM3S9B96

Hi all, 

 in my Project i use a Keil uVision (v. 4.60.0.0)  and a Keil ULink2-Jtag-adapter. The Jtag is only connected to one LM3S9B96. The Debugger detect an ARM CoreSight JTAG-DP (IDCODE 0x4BA00477; IR len 4 on AP 0x00) 

Since today I get the error message "Invalid ROM Table"

In uVison I tested various debug settings.
(Alt + F7 -> Debug -> Debugger (ULINK2/ME Cortex Debugger) -> Settings -> Reset Options & Connect: Connect and rest).
Unfortunately, I can not reprogram the controller.

Are there any other settings that I can try.

Thanks, Frank