https://support.ti.com/csm sent me to this forum. Odd when the "TM4C129ENCPDTT3" part number is entered in the form to create this entry it reports 'unknown part number' But the API appears to beware of the part number.
On November 4, 2022 10 pieces of part number "TM4C129ENCPDTT3" a powershell script placed an order using the URL "
https://transact.ti.com/v2/store/orders" (a secure token was acquired and provided with the following json:
{ "order":
{
"checkoutProfileId": "****",
"customerPurchaseOrderNumber": "Sukhy",
"endCustomerCompanyName": "Telecor Inc.",
"expediteShipping": false,
"customerOrderComments": [
{
"message": "automated order from Telecor Inc Canada"
}
],
"lineItems": [
{
"customerLineItemNumber": 1,
"tiPartNumber": "TM4C129ENCPDTT3",
"customerPartNumber": "",
"customReelIndicator": false,
"quantity": 1,
"customerItemComments": [
{
"message": "auto ordered"
}
]
}
]
}
}
However the following response was received:
{
"errors" : [
{
"errorCode" : "ERR-TICOM-ORDER-API-GEN-0500",
"section" : "Generic",
"type" : "Validation",
"reason" : "We encountered a technical issue in processing your request.",
"message" : "The API is temporarily unavailable. Please retry, if the issue persists, Please contact TI customer support - https://support.ti.com/csm"
}
]
}
This lasted for 3 days until Nov 7, 2022 when the pieces were no longer available. I have tried stepping through the powershell code and now with 0 available if the order is placed The following response is observed
errorCode : ERR-TICOM-ORDER-API-0001
type : lineItems
section : Orders
field :
reason : Part number(s) requested inventory quantity is not available per your request
message : Please check the inventory levels for available quantity and resubmit the request with different qty. Note In instances of low inventory ordering limits may be set
data : {@{customerLineItemNumber=1; tiPartNumber=TM4C129ENCPDTT3; quantity=1; availableQuantity=0; limit=999999999}}
Placing the same order on the test site has the same result for part number TM4C129ENCPDTT3 and a success if the part number is changed to NE555DR.
The concern I have is that there is something not right with the order request that is causing the "ERR-TICOM-ORDER-API-GEN-0500" to be generated. But it looks like the server is throwing an exception on the request. This issue persisted for 3 days until Nov 7, 2022. Is there something not right with the request?
Thank you,