hi,
I need a buck conver with the following specifications.
1. Input Volt = 24 to 48 V
2. Output Volt = 1V
3. output current = 100 to150 A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anand,
Take a look at the LM25143 two-phase controller. Two ICs can be used to create a 4-phase solution (25A to 37.5A per phase). You can use the quickstart calculator or WEBENCH to assist with component selection.
Regards,
Tim
**Attention** This is a public forum