Other Parts Discussed in Thread: ADS127L21
Tool/software:
Hi,
In a related question, I was informed that you will release C code to control the EVM board programmatically by the end of the year (2024).
What's the status on this? I don't see anything online.
Furthermore, I see that from the GUI that I can manipulate the sampling rate down to 8kHz. But this is done by using the Clock divider in the internal interface to Div/16 and then by also dividing the external clock (EVM CLK) by a factor of 2 (or the opposite, 16 in the External clock and 2 in the clock divider in the internal interface option).
How can I do that programmatically? I am interested in a sampling rate <32kHz which requires a division of both clocks. I have checked the github repository for the ADS127L11EVM board (previous version), and there is no mention of an external clock, at least up to my understanding of the code.
Kind regards,
Vasilis