Hi Team
My customer is developing 947 <->948 for CID application.
now they met some issue that
when they test 947 with their tester display module with 948, 0x0c bit[0] is high and display is OK.
but when they test 947 with customer display module with 948 0x0c bit[0] is low and display also OK. and customer cannot access to DES via BCC.
As I experienced from 949, if Link detect status is failed, HDMI Input port was not enabled. so display was NG.
Does device enable OLDI port input even Link detect status (0x0c bit[0]=1b'0 ) is low?? so this doesn't care Link detect status for outputting data on Link channel??
Thanks~